UserDefinedEvent Class

class NXOpen.UserDefinedObjects.UserDefinedEvent

Bases: NXOpen.TransientObject

Implements the Event Object for UDO’s

New in version NX5.0.0.

Properties

Property Description
EventReason Returns the reason we fired this event.
UserDefinedObject Returns the related UDO.

Methods

Method Description
Dispose Frees the object from memory.

Enumerations

UserDefinedEventReason Enumeration Available link types for a UserDefinedObject.

Property Detail

EventReason

UserDefinedEvent.EventReason

Returns the reason we fired this event.

-------------------------------------

Getter Method

Signature EventReason()

Returns:The reason for the event
Return type:NXOpen.UserDefinedObjects.UserDefinedEventReason

New in version NX5.0.0.

License requirements: None.

UserDefinedObject

UserDefinedEvent.UserDefinedObject

Returns the related UDO.

-------------------------------------

Getter Method

Signature UserDefinedObject()

Returns:The UDO that caused the event to fire
Return type:NXOpen.UserDefinedObjects.UserDefinedObject

New in version NX5.0.0.

License requirements: None.

Method Detail

Dispose

UserDefinedEvent.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET and Java, his method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX5.0.0.

License requirements: None.