UserDefinedEventReason Enumeration

NXOpen.UserDefinedObjects.UserDefinedEvent.Reason is an alias for NXOpen.UserDefinedObjects.UserDefinedEventReason

class NXOpen.UserDefinedObjects.UserDefinedEventReason

Bases: object

Available link types for a UserDefinedObject.

Enum Members

Enum Member Enum Member Description
Display
Display UDO event
Delete
An associated object was deleted - UDO cleanup event
Update
Update UDO event
Selection
Select UDO event
Fit
Fit display event
AttentionPoint
Find Attention Point for the UDO event
Info
Query UDO Information event
Edit
Edit UDO event
Suppress
Suppress/Unsuppress UDO event
ScreenSizeFit
Fit operation for screen-size geometry
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.