StylerEvent Class

class NXOpen.UIStyler.StylerEvent

Bases: NXOpen.TransientObject

Represents a StylerEvent

New in version NX5.0.0.

Methods

Method Description
Dispose Free resources associated with the instance.
GetReason Gets the reason for the event @return Reason
GetStylerItem Gets the dialog item @return

Enumerations

StylerEventIndicator Enumeration Describes indicator value
StylerEventMiscellaneous Enumeration Describes event index
StylerEventReason Enumeration Describes callback reason

Method Detail

Dispose

StylerEvent.Dispose

Free resources associated with the instance.

After this method is called, it is illegal to use the object. In .NET or Java, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX5.0.0.

License requirements: None.

GetReason

StylerEvent.GetReason

Gets the reason for the event

Signature GetReason()

Returns:Reason
Return type:NXOpen.UIStyler.StylerEventReason

New in version NX5.0.0.

License requirements: None.

GetStylerItem

StylerEvent.GetStylerItem

Gets the dialog item

Signature GetStylerItem()

Returns:
Return type:NXOpen.UIStyler.StylerItem

New in version NX5.0.0.

License requirements: None.