StylerEventReason Enumeration¶
NXOpen.UIStyler.StylerEvent.Reason is an alias for NXOpen.UIStyler.StylerEventReason
-
class
NXOpen.UIStyler.
StylerEventReason
¶ Bases:
object
Describes callback reason
Enum Members
Enum Member Enum Member Description NoReason No reasonActivateReason Activate reasonValueChangedReason Value changed reasonDragReason Drag reasonDoubleClickReason Double click reasonOkReason Ok reasonApplyReason Apply reasonBackReason BAck reasonCancelReason Cancel reasonConstructReason Construct reasonDestructReason Destruct reasonFileopReason File operation reasonSwitchReason Switch reasonFileOperationReason File operation reasonExitFileOperationReason Exit file operation reason-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-