NXOpen.UF.Weight.SetPartMaxWeight¶
-
Weight.
SetPartMaxWeight
()¶ Refer to UF_WEIGHT_set_part_max_weight for documentation.
Signature:
SetPartMaxWeight(part, maxWeight, units)
Parameters: - part (Tag) – The part whose maximum weight limit is to be set.
- maxWeight (float) – The value of the new maximum weight limit for the part.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the maximum weight limit is expressed.
License requirements: ADVANCED ASSEMBLIES