UF_WEIGHT_exception_reason_e (view source)
Defined in: uf_weight.h
Also known as:
- UF_WEIGHT_exception_reason_t
- UF_WEIGHT_exception_reason_p_t
Overview
Values for the different exceptions that can be generated while
calculating weight data.
Data Members
UF_WEIGHT_not_loaded = 1
UF_WEIGHT_insufficiently_loaded = 2
UF_WEIGHT_ref_set_absent = 3
UF_WEIGHT_comp_set_absent = 4
UF_WEIGHT_under_minimum_weight = 8
UF_WEIGHT_over_maximum_weight = 9
UF_WEIGHT_has_assertion = 11
UF_WEIGHT_insufficient_accuracy = 12
UF_WEIGHT_incomplete_part = 15
UF_WEIGHT_comp_group_not_uptodate = 16
UF_WEIGHT_comp_group_updated_successfully = 17
UF_WEIGHT_reference_only_component = 18
UF_WEIGHT_excluded_from_spatial_search = 19
UF_WEIGHT_promotion_with_source_suppressed = 20
UF_WEIGHT_state_type_e (view source)
Defined in: uf_weight.h
Also known as:
- UF_WEIGHT_state_type_t
- UF_WEIGHT_state_type_p_t
Overview
Values for weight property states.
Data Members
UF_WEIGHT_no_cache = 0
UF_WEIGHT_cached = 1
UF_WEIGHT_asserted = 2
UF_WEIGHT_unknown = 3
UF_WEIGHT_inherited = 4
UF_WEIGHT_implied = 6
UF_WEIGHT_units_type_e (view source)
Defined in: uf_weight.h
Also known as:
- UF_WEIGHT_units_type_t
- UF_WEIGHT_units_type_p_t
Overview
Enum for possible units of mass and length for weight properties.
Data Members
UF_WEIGHT_units_km = 0
UF_WEIGHT_units_li
UF_WEIGHT_units_lf
UF_WEIGHT_units_gm
UF_WEIGHT_units_gc
UF_WEIGHT_units_custom
UF_WEIGHT_units_kmm
cached properties are not available for
it.