NXOpen.UF.Weight.EstabSolidProps¶
-
Weight.
EstabSolidProps
()¶ Refer to UF_WEIGHT_estab_solid_props for documentation.
Signature:
EstabSolidProps(solid, accuracy, units)
Parameters: - solid (Tag) – The solid whose properties are to be calculated.
- accuracy (float) – The accuracy to which the solid’s properties are to be calculated.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the properties are to be returned.
Returns: The established properties of the solid.
Return type: NXOpen.UF.Weight.Properties
Refer to UF_WEIGHT_properties_s for documentation.License requirements: ADVANCED ASSEMBLIES