NXOpen.UF.Weight.EstabPartProps¶
-
Weight.
EstabPartProps
()¶ Refer to UF_WEIGHT_estab_part_props for documentation.
Signature:
EstabPartProps(part, accuracy, recurse, units)
Parameters: - part (Tag) – The part whose weight properties are to be established.
- accuracy (float) – The accuracy to which the part’s properties are to be calculated.
- recurse (bool) – True if the properties are to include components of the part, false otherwise.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the properties are to be returned.
Returns: A Tuple
Return type: A tuple consisting of (properties,exceptions)
properties(
`NXOpen.UF.Weight.Properties
Refer to UF_WEIGHT_properties_s for documentation.`): The established properties of the part.exceptions(
`NXOpen.UF.Weight.Exceptions
Refer to UF_WEIGHT_exceptions_s for documentation.`): Any exceptions encountered during the calculation. This must be freed by calling UF_WEIGHT_free_exceptions.License requirements: ADVANCED ASSEMBLIES