NXOpen.UF.Weight.EstabCompProps¶
-
Weight.
EstabCompProps
()¶ Refer to UF_WEIGHT_estab_comp_props for documentation.
Signature:
EstabCompProps(component, accuracy, recurse, units)
Parameters: - component (Tag) – The component whose properties are to be calculated.
- accuracy (float) – The accuracy to which the component’s properties are to be calculated.
- recurse (bool) – True if the properties are to include the component’s child components, false otherwise.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the properties are to be returned.
Returns: A Tuple
Return type: A tuple consisting of (properties,exceptions)
properties(
`NXOpen.UF.Weight.Properties
Refer to UF_WEIGHT_properties_s for documentation.`): The established properties of the component.exceptions(
`NXOpen.UF.Weight.Exceptions
Refer to UF_WEIGHT_exceptions_s for documentation.`): Any exceptions encountered during the calculation. This structure must be freed by calling UF_WEIGHT_free_exceptionsLicense requirements: ADVANCED ASSEMBLIES