NXOpen.UF.Weight.AskProps¶
-
Weight.
AskProps
()¶ Refer to UF_WEIGHT_ask_props for documentation.
Signature:
AskProps(objectArg, units)
Parameters: - objectArg (Tag) – Part, component or solid body whose weight properties are wanted.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the properties are to be returned.
Returns: The current properties of object.
Return type: NXOpen.UF.Weight.Properties
Refer to UF_WEIGHT_properties_s for documentation.License requirements: None