NXOpen.UF.Weight.AskPartMinWeight¶
-
Weight.
AskPartMinWeight
()¶ Refer to UF_WEIGHT_ask_part_min_weight for documentation.
Signature:
AskPartMinWeight(part, units)
Parameters: - part (Tag) – The part whose minimum weight limit is to be returned.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the minimum weight limit is to be expressed.
Returns: A Tuple
Return type: A tuple consisting of (minWeight,isSet)
minWeight(float): The value of the minimum weight limit of part (0.0 if the limit is not set).
isSet(bool): True if the minimum weight limit of the part is currently set, false if not.
License requirements: None