NXOpen.UF.Weight.AskPartMaxWeight¶
-
Weight.
AskPartMaxWeight
()¶ Refer to UF_WEIGHT_ask_part_max_weight for documentation.
Signature:
AskPartMaxWeight(part, units)
Parameters: - part (Tag) – The part whose maximum weight limit is to be returned.
- units (
NXOpen.UF.Weight.UnitsType
Refer to UF_WEIGHT_units_type_e for documentation.) – The units in which the maximum weight limit is to be expressed.
Returns: A Tuple
Return type: A tuple consisting of (maxWeight,isSet)
maxWeight(float): The value of the maximum weight limit of part (0.0 if the limit is not set).
isSet(bool): True if the maximum weight limit of the part is currently set, false if not.
License requirements: None