NXOpen.UF.Uf.SystemInfo Structure¶
NXOpen.UF.Uf.SystemInfo is an alias for NXOpen.UF.UfSystemInfo_Struct
-
class
NXOpen.UF.
UfSystemInfo_Struct
¶ Bases:
object
Refer to UF_system_info_s for documentation.
Fields
NXOpen.UF.UfSystemInfo_Struct.DateBuf |
Current date and time info |
NXOpen.UF.UfSystemInfo_Struct.UserName |
User, who is running this process |
NXOpen.UF.UfSystemInfo_Struct.ProgramName |
The current program name |
NXOpen.UF.UfSystemInfo_Struct.NodeName |
Machine, on which this process is running |
NXOpen.UF.UfSystemInfo_Struct.MachineType |
Hardware type on which the machine is running |
NXOpen.UF.UfSystemInfo_Struct.OsName |
Operating system, on which this process is running |
NXOpen.UF.UfSystemInfo_Struct.OsVersion |
Version and release level of this Operating System |
NXOpen.UF.UfSystemInfo_Struct.PhysicalMemory |
Returns the number of bytes of physical memory on this machine. |
NXOpen.UF.UfSystemInfo_Struct.BundlesUsed |
Array of the names of the bundles currently in use. |
NXOpen.UF.UfSystemInfo_Struct.NumberOfBundles |
The number of bundles currently in use |