UF_system_info_s (view source)
Defined in: uf.h
Also known as:
- UF_system_info_t
- UF_system_info_p_t
Overview
The structure UF_system_info_t below is used to get the information about
the current process. The routine UF_ask_system_info retrieves the
information about the process and fills the structure. Once the data is used,
the memory allocated to these fields should be freed by calling the routine,
UF_free_system_info.
Data Members
date_buf
char *
user_name
char *
program_name
char *
node_name
char *
machine_type
char *
os_name
char *
os_version
char *
physical_memory
long
bundles_used
char * *
number_of_bundles
int