NXOpen.UF.Sket.ConGeom Structure¶
NXOpen.UF.Sket.ConGeom is an alias for NXOpen.UF.SketConGeom_Struct
-
class
NXOpen.UF.
SketConGeom_Struct
¶ Bases:
object
Refer to UF_SKET_con_geom_s for documentation.
Fields
NXOpen.UF.SketConGeom_Struct.GeomTag |
The geomtry’s tag |
NXOpen.UF.SketConGeom_Struct.VertexType |
Vertex type if it is the vertex of the geometry that will be constrained. |
NXOpen.UF.SketConGeom_Struct.VertexIndex |
Starting from 1. |
NXOpen.UF.SketConGeom_Struct.UseHelp |
Whether to use help data (either help points or help parameter.) Valid types as specified in UF_SKET_help_type_t. |
NXOpen.UF.SketConGeom_Struct.HelpPoint |
Help point |
NXOpen.UF.SketConGeom_Struct.HelpParameter |
Help parameter |