NXOpen.UF.SketConGeom_Struct.UseHelp¶
-
SketConGeom_Struct.
UseHelp
¶ Whether to use help data (either help points or help parameter.) Valid types as specified in UF_SKET_help_type_t. Help points/parameters are used to indicate whereabouts on the geometry a constraint should apply to. They are only needed when the constraints are of type UF_SKET_tangent, UF_SKET_point_on_curve, or UF_SKET_point_on_string.