NXOpen.UF.SfUgsTetMeshParms_Struct.ElementType |
Desired element type. |
NXOpen.UF.SfUgsTetMeshParms_Struct.Midnodes |
TRUE for tet10s,FALSE for tet4s. |
NXOpen.UF.SfUgsTetMeshParms_Struct.ElementSize |
Desired element size. |
NXOpen.UF.SfUgsTetMeshParms_Struct.MidnodeOption |
Whether to project midnodes or not. |
NXOpen.UF.SfUgsTetMeshParms_Struct.GeometryToleranceToggle |
Geometry Tolerance for midnode straightening |
NXOpen.UF.SfUgsTetMeshParms_Struct.GeometryToleranceValue |
Geometry Tolerance value for midnode straightening |
NXOpen.UF.SfUgsTetMeshParms_Struct.MaximumMidnodeJacobian |
If midnode_option = UF_SF_UGS_MESHER_mixed_midnodes, any element with a jacobian value higher than maximum_midnode_jacobian will have its midnodes straightened. |
NXOpen.UF.SfUgsTetMeshParms_Struct.MinimumFaceAngle |
Minimum angle at corner of a face that can support element. |
NXOpen.UF.SfUgsTetMeshParms_Struct.SurfMeshSizeVariation |
This controls how much variation in element size is desired/permitted in the mesh on the surface of the bodies being meshed. |
NXOpen.UF.SfUgsTetMeshParms_Struct.TetMeshSizeVariation |
This controls whether the tets are permitted to expand as you progress into the interior of the body. |
NXOpen.UF.SfUgsTetMeshParms_Struct.MultiBlockDecomposition |
Attempt MultiBlock Decomposition 0=OFF,1=ON |
NXOpen.UF.SfUgsTetMeshParms_Struct.MeshTransition |
Mesh transition 0=OFF,1=ON |
NXOpen.UF.SfUgsTetMeshParms_Struct.RemeshToggle |
Avoid failing elements by reducing element size 0=OFF,1=ON |
NXOpen.UF.SfUgsTetMeshParms_Struct.CreatePyramids |
Create pyramid transition elements. |
NXOpen.UF.SfUgsTetMeshParms_Struct.SmallFeature |
% of element length for abstraction |
NXOpen.UF.SfUgsTetMeshParms_Struct.AttemptMappedMeshing |
|
NXOpen.UF.SfUgsTetMeshParms_Struct.TwoElementThroughThicknessToggle |
|
NXOpen.UF.SfUgsTetMeshParms_Struct.AutoFixFailedElementsToggle |
|
NXOpen.UF.SfUgsTetMeshParms_Struct.EdgeMergeToggle |
Edge merge toggle 0 or 1 |
NXOpen.UF.SfUgsTetMeshParms_Struct.EdgeAngle |
Edge merge angle |
NXOpen.UF.SfUgsTetMeshParms_Struct.FilletToggle |
true => Filler detection ON false=> Fillet detection OFF |
NXOpen.UF.SfUgsTetMeshParms_Struct.FilletType |
Used only if fillet_toggle == true Fillet type |
NXOpen.UF.SfUgsTetMeshParms_Struct.FilletNumElem |
No of elements on a quarter arc of fillet |
NXOpen.UF.SfUgsTetMeshParms_Struct.FilletMinRad |
Min radius |
NXOpen.UF.SfUgsTetMeshParms_Struct.FilletMaxRad |
|