NXOpen.UF.SfUgsTetMeshParms_Struct.SurfMeshSizeVariation¶
-
SfUgsTetMeshParms_Struct.
SurfMeshSizeVariation
¶ This controls how much variation in element size is desired/permitted in the mesh on the surface of the bodies being meshed. Valid values go from 0 to 100. This number does not coorespond directly to any actual meshing parameter, but rather is a relative scale that the user can use to indicate their tolerance for mesh variation. It is used internally in the mesher to calculate expansion factors and a minimum element size. 0 means that there will be minimumal element size variation. 100 means that there will be maximum element size variation.