NXOpen.UF.Sflegend.IndexAttr StructureΒΆ
NXOpen.UF.Sflegend.IndexAttr is an alias for NXOpen.UF.SfLegendIndexAttr_Struct
Fields
NXOpen.UF.SfLegendIndexAttr_Struct.AttrMask |
This field is set to one or more of the following symbols OR’d together to indicate which of the remaining fields of the structure are set. |
NXOpen.UF.SfLegendIndexAttr_Struct.HeightPercent |
The percentage of the legend area which the index fills. |
NXOpen.UF.SfLegendIndexAttr_Struct.ColorAttr |
The attributes of the color index default: none specified |
NXOpen.UF.SfLegendIndexAttr_Struct.TextAttr |
The attributes of the text index If not specified, default labeling will be used for the color index. |