SfLegendIndexAttr_Struct.
HeightPercent
The percentage of the legend area which the index fills. The index is placed in the middle of the legend unless there is a long header in which case the index follows directly after. default: 50%