NXOpen.UF.Sf.EdgeDensityData Structure¶
NXOpen.UF.Sf.EdgeDensityData is an alias for NXOpen.UF.SfEdgeDensityData_Struct
-
class
NXOpen.UF.
SfEdgeDensityData_Struct
¶ Bases:
object
Refer to UF_SF_edge_density_data_s for documentation.
Fields
NXOpen.UF.SfEdgeDensityData_Struct.Type |
indicates the type of density (size or number). |
NXOpen.UF.SfEdgeDensityData_Struct.Size |
The number of elements on the edge/curve is calculated automatically from the length of the edge/curve and the element size. |
NXOpen.UF.SfEdgeDensityData_Struct.Number |
The number of elements on the edge/curve is calculated automatically from the length of the edge/curve and the element size. |