SfEdgeDensityData_Struct.
Number
The number of elements on the edge/curve is calculated automatically from the length of the edge/curve and the element size. If this option is set, the value of number is disregarded.