NXOpen.UF.Scop.VectorData Structure¶
NXOpen.UF.Scop.VectorData is an alias for NXOpen.UF.ScopVectorData_Struct
-
class
NXOpen.UF.
ScopVectorData_Struct
¶ Bases:
object
Refer to UF_SCOP_vector_data_s for documentation.
Fields
NXOpen.UF.ScopVectorData_Struct.Xyz |
the vector location |
NXOpen.UF.ScopVectorData_Struct.Ijk |
the vector direction, if data type is UF_SCOP_TX_INTP_DATYPE_VECTOR |
NXOpen.UF.ScopVectorData_Struct.LeadTilt |
the vector lead angle and tilt angle, if data type is UF_SCOP_TX_INTP_DATYPE_ANGLE_DS or UF_SCOP_TX_INTP_DATYPE_ANGLE_PS |
NXOpen.UF.ScopVectorData_Struct.IsCornerVector |
If TRUE, this vector can not be deleted. |