NXOpen.UF.ScopVectorData_Struct.IsCornerVector¶
-
ScopVectorData_Struct.
IsCornerVector
¶ If TRUE, this vector can not be deleted. The users must set a vector on each corner of the Drive surface. (Therefore, four vectors must be set to the Drive surface, one for each corner. Two vectors must be set to Curve/Point method.) The flags “is_corner_vector” of these vectors must be set to TRUE.