NXOpen.UF.Obj.CycleTypedObjsInPart¶
-
Obj.
CycleTypedObjsInPart
()¶ Refer to UF_OBJ_cycle_typed_objs_in_part for documentation.
Signature:
CycleTypedObjsInPart(partTag, type, objectArg)
Parameters: - partTag (Tag) – Tag of part you wish to cycle
- type (int) – Type of object on which to cycle
- objectArg (Tag) – On input the object found by the last call to this routine. if this routine has not been called yet, then set object=NULL_TAG to start cycling. On output the next object of the type specified. If there is no object, and the cycling is complete a NULL_TAG is returned.
Returns: Modified value of objectArg
Return type: License requirements: None