NXOpen.UF.Obj.CycleByNameAndType¶
-
Obj.
CycleByNameAndType
()¶ Refer to UF_OBJ_cycle_by_name_and_type for documentation.
Signature:
CycleByNameAndType(partTag, name, type, useOcc, objectArg)
Parameters: - partTag (Tag) – Tag of part in which to cycle.
- name (str) – Name of objects on which to cycle.
- type (int) – Object type on which to cycle (see uf_object_types.h)
- useOcc (bool) – Occurrence filter: TRUE = include occurrences FALSE = exclude occurrrences
- objectArg (Tag) – On input the object found by the last call to this routine. Begin the cycle by passing in object = NULL_TAG On output, the next object of the given name. Outputs a NULL_TAG when the cycle is finished.
Returns: Modified value of objectArg
Return type: License requirements: None