NXOpen.UF.Obj.AskTranslucency¶
-
Obj.
AskTranslucency
()¶ Refer to UF_OBJ_ask_translucency for documentation.
Signature:
AskTranslucency(objectArg)
Parameters: objectArg (Tag) – The object for which you are asking the translucency It must be of one of the following types: UF_solid_type, with one of these subtypes: UF_solid_body_type UF_solid_face_type UF_faceted_model_type UF_component_type Returns: percent translucent 0 - 100 Return type: int License requirements: None