NXOpen.UF.Motion.VectorForceTorque Structure¶
NXOpen.UF.Motion.VectorForceTorque is an alias for NXOpen.UF.MotionVectorForceTorque_Struct
-
class
NXOpen.UF.
MotionVectorForceTorque_Struct
¶ Bases:
object
Refer to UF_MOTION_vector_force_torque_s for documentation.
Fields
NXOpen.UF.MotionVectorForceTorque_Struct.Name |
The name of the force or torque. |
NXOpen.UF.MotionVectorForceTorque_Struct.Vtype |
Either UF_MOTION_vector_force or UF_MOTION_vector_torque. |
NXOpen.UF.MotionVectorForceTorque_Struct.Link |
The link that the force or torque is acting on. |
NXOpen.UF.MotionVectorForceTorque_Struct.Origin |
The point that defines the location the force or torque is acting on. |
NXOpen.UF.MotionVectorForceTorque_Struct.Direction |
The vector that defines the orientation of the force or torque if reference frame is UF_MOTION_first_link. |
NXOpen.UF.MotionVectorForceTorque_Struct.Frame |
The reference frame of the force or torque: UF_MOTION_absolute means the orientation of the force/torque is constant with respect to the absolute CSYS regardless of the motion of the link. |
NXOpen.UF.MotionVectorForceTorque_Struct.CompFunctions |
For reference frame of UF_MOTION_absolute: The functions describing the X, Y, and Z components of the force or torque. |
NXOpen.UF.MotionVectorForceTorque_Struct.MagnitudeFunction |
For reference frame of UF_MOTION_first_link: A single function tag describing the force or torque magnitude. |
NXOpen.UF.MotionVectorForceTorque_Struct.ReactionLink |
The optional link that receives an equal and opposite reaction force or torque. |