NXOpen.UF.ModlSymbThreadData_Struct.CylFace |
Cylindrical face to be threaded. |
NXOpen.UF.ModlSymbThreadData_Struct.StartFace |
Face at which the thread starts. |
NXOpen.UF.ModlSymbThreadData_Struct.AxisDirection |
Direction of the thread. |
NXOpen.UF.ModlSymbThreadData_Struct.IncludeInstances |
Instancing flag, UF_MODL_NO_INSTANCES means no thread on instances of cylindrical face. |
NXOpen.UF.ModlSymbThreadData_Struct.Rotation |
Rotation, either UF_MODL_RIGHT_HAND or UF_MODL_LEFT_HAND. |
NXOpen.UF.ModlSymbThreadData_Struct.LengthFlag |
Indicates the thread is a fixed length or a full thread. |
NXOpen.UF.ModlSymbThreadData_Struct.Tapered |
UF_MODL_TAPERED if this is a tapered thread, UF_MODL_NON_TAPERED if this is a non tapered thread. |
NXOpen.UF.ModlSymbThreadData_Struct.NumStarts |
Number of start. |
NXOpen.UF.ModlSymbThreadData_Struct.Length |
Expression of the thread length. |
NXOpen.UF.ModlSymbThreadData_Struct.Form |
Thread form. |
NXOpen.UF.ModlSymbThreadData_Struct.Method |
Thread method. |
NXOpen.UF.ModlSymbThreadData_Struct.Callout |
Thread callout. |
NXOpen.UF.ModlSymbThreadData_Struct.MajorDia |
Major diameter expression of the thread. |
NXOpen.UF.ModlSymbThreadData_Struct.MinorDia |
Minor diameter expression of the thread. |
NXOpen.UF.ModlSymbThreadData_Struct.TappedDia |
Tapped diameter expression of the thread. |
NXOpen.UF.ModlSymbThreadData_Struct.Pitch |
Thread pitch expression. |
NXOpen.UF.ModlSymbThreadData_Struct.Angle |
Thread angle expression. |
NXOpen.UF.ModlSymbThreadData_Struct.InternalThread |
Indicates type of thread. |