NXOpen.UF.ModlSymbThreadData_Struct.Callout¶
-
ModlSymbThreadData_Struct.
Callout
¶ Thread callout. In creation, if you specify a callout, the major diameter, minor diameter, pitch, tapped drill/shaft diameter, length, and tapered indicator are read from the thread table and the values of those parameters from the structure are ignored except for the length value. If the length value is specified in the structure, it will be used instead of the one read from the table. If no callout is specified, the values of those parameters are used in creating the thread. Not specifying a callout means to pass a NULL pointer, passing an empty string (“”) causes an error. In Inquiry, if a callout is specified in creating the thread, those parameters also return in the structure together with the callout.