NXOpen.UF.Facet.Parameters Structure¶
NXOpen.UF.Facet.Parameters is an alias for NXOpen.UF.FacetParameters_Struct
-
class
NXOpen.UF.
FacetParameters_Struct
¶ Bases:
object
Refer to UF_FACET_parameters_s for documentation.
Fields
NXOpen.UF.FacetParameters_Struct.Version |
The version of this structure. |
NXOpen.UF.FacetParameters_Struct.MaxFacetEdges |
The maximum number of edges allowed in the facets that are to be generated. |
NXOpen.UF.FacetParameters_Struct.SpecifySurfaceTolerance |
If this value is true, then values must be specified for surface_dist_tolerance and surface_angular_tolerance. |
NXOpen.UF.FacetParameters_Struct.SurfaceDistTolerance |
This is the maximum distance from the surface to the facet. |
NXOpen.UF.FacetParameters_Struct.SurfaceAngularTolerance |
This is the maximum angular variation in radians of the surface normal over the facet. |
NXOpen.UF.FacetParameters_Struct.SpecifyCurveTolerance |
This indicates that values are to be specified for curve_dist_tolerance and curve_angular_tolerance and curve_max_length. |
NXOpen.UF.FacetParameters_Struct.CurveDistTolerance |
This is the maximum distance between the facet edge and the curve segment represented by the facet edge. |
NXOpen.UF.FacetParameters_Struct.CurveAngularTolerance |
This is the maximum angular variation in radians of the curve tangent along the curve segment represented by the facet edge. |
NXOpen.UF.FacetParameters_Struct.CurveMaxLength |
|
NXOpen.UF.FacetParameters_Struct.SpecifyConvexFacets |
This indicates that the facets generated by the faceter should all be convex |
NXOpen.UF.FacetParameters_Struct.SpecifyMaxFacetSize |
This indicates that a maximum width of facet is to be specified using max_facet_size. |
NXOpen.UF.FacetParameters_Struct.MaxFacetSize |
This is the maximum width of a facet. |
NXOpen.UF.FacetParameters_Struct.NumberStorageType |
This indicates whether the real numbers for facet vertices and facet normals should be stored as floats (UF_FACET_TYPE_FLOAT) or as doubles (UF_FACET_TYPE_DOUBLE). |
NXOpen.UF.FacetParameters_Struct.SpecifyParameters |
This indicates that the model will be created with the parametric information for each vertex. |
NXOpen.UF.FacetParameters_Struct.SpecifyViewDirection |
Should we use a viewing direction for denser faceting around silhouettes. |
NXOpen.UF.FacetParameters_Struct.SilhViewDirection |
If use_view_direction is specified, then this is the view direction to use. |
NXOpen.UF.FacetParameters_Struct.SilhChordTolerance |
If use_view_direction is specified then this is the tolerance which will be used as a tighter surface tolerance in the silhouette area specified by the view direction. |
NXOpen.UF.FacetParameters_Struct.StoreFaceTags |
Should this FACET body record face tags or not. |