NXOpen.UF.FacetParameters_Struct.SpecifyCurveTolerance¶
-
FacetParameters_Struct.
SpecifyCurveTolerance
¶ This indicates that values are to be specified for curve_dist_tolerance and curve_angular_tolerance and curve_max_length. If this value is false then values for curve_dist_tolerance and curve_angular_tolerance will be determined by the system based on the body box or face box of the solid entity being faceted, and no restriction will be placed on the maximum length of curve that can be represented by a single facet edge.