NXOpen.UF.Disp.ExportWindowsMetafile¶
-
Disp.
ExportWindowsMetafile
()¶ Refer to UF_DISP_export_windows_metafile for documentation.
Signature:
ExportWindowsMetafile(outputType, fileSpec)
Parameters: - outputType (
NXOpen.UF.Disp.WmfOutput
Refer to UF_DISP_wmf_output_e for documentation.) – Specifies where the output Enhanced Metafile should be written: UF_DISP_WMF_TO_CLIPBOARD writes directly to the Windows clipboard. This is not available in external NX Open programs. UF_DISP_WMF_TO_FILE uses the following file_spec to output the metafile data to. - fileSpec (str) – The file specification of the file to create. This parameter is used only when the output_type is UF_DISP_WMF_TO_FILE. This file specification must be at most MAX_FSPEC_SIZE characters.
License requirements: None
- outputType (