NXOpen.UF.Disp.DisplayTemporaryText¶
-
Disp.
DisplayTemporaryText
()¶ Refer to UF_DISP_display_temporary_text for documentation.
Signature:
DisplayTemporaryText(viewTag, whichViews, text, textCoord, refPoint, color, charSize, hardware)
Parameters: - viewTag (Tag) – The tag of the view in which to display the temporary text.
- whichViews (
NXOpen.UF.Disp.ViewType
Refer to UF_DISP_view_type_e for documentation.) – The view mode to use. - text (list of str) – Lines of text
- textCoord (list of float) – Position of text box reference point in absolute coordinates of the displayed part.
- refPoint (
NXOpen.UF.Disp.TextRef
Refer to UF_DISP_text_ref_e for documentation.) – Reference point of text box - color (
NXOpen.UF.Obj.DispProps
Refer to UF_OBJ_disp_props_s for documentation.) – The color element of the structure. All other elements of the structure are ignored. If color->color = 0, then the system default color is used. - charSize (float) – The character size in part units (Metric or inches). Used only if software text is used. If
- hardware (int) – hardware/software flag: 0 = Use hardware font 1 = Use software font
License requirements: None