NXOpen.UF.Disp.DisplayTemporaryPoint¶
-
Disp.
DisplayTemporaryPoint
()¶ Refer to UF_DISP_display_temporary_point for documentation.
Signature:
DisplayTemporaryPoint(viewTag, whichViews, markerpos, color, markerType)
Parameters: - viewTag (Tag) – The tag of the view in which to display the temporary maker.
- whichViews (
NXOpen.UF.Disp.ViewType
Refer to UF_DISP_view_type_e for documentation.) – The view mode to use. - markerpos (list of float) – The marker position in absolute coordinates of the work part
- color (
NXOpen.UF.Obj.DispProps
Refer to UF_OBJ_disp_props_s for documentation.) – The color element of the structure. All other elements of the structure are ignored. If color->color = 0, then the system default color is used. - markerType (
NXOpen.UF.Disp.PolyMarker
Refer to UF_DISP_poly_marker_e for documentation.) – The marker type
License requirements: None