NXOpen.UF.Disp.DisplayTemporaryArc¶
-
Disp.
DisplayTemporaryArc
()¶ Refer to UF_DISP_display_temporary_arc for documentation.
Signature:
DisplayTemporaryArc(viewTag, whichViews, matrix, startAngle, endAngle, arcCenter, radius, attrib)
Parameters: - viewTag (Tag) – The tag of the view in which to display the temporary arc.
- whichViews (
NXOpen.UF.Disp.ViewType
Refer to UF_DISP_view_type_e for documentation.) – The view mode to use. - matrix (list of float) – A matrix for the CSYS in which the arc exists. Use UF_MTX3_initialize to create a matrix from X and Y vectors.
- startAngle (float) – Start angle in radians
- endAngle (float) – End angle in radians.
- arcCenter (list of float) – Coordinates are with respect to the CSYS of the matrix in the work part.
- radius (float) – Radius from the arc center.
- attrib (
NXOpen.UF.Obj.DispProps
Refer to UF_OBJ_disp_props_s for documentation.) – The color, font, and width elements of the structure should be set to: attrib->color = color index attrib->font = 1 for solid 2-7, user defined 0 use system default attrib->line_width = line width values in uf_obj.h -1 use the default width
License requirements: None