NXOpen.UF.Disp.DisplaySketDimensions¶
-
Disp.
DisplaySketDimensions
()¶ Refer to UF_DISP_display_sket_dimensions for documentation.
Signature:
DisplaySketDimensions(sketchTag, expCount, expTags, viewOption, colorOption, color)
Parameters: - sketchTag (Tag) – Tag of the sketch to which the dimensions belong
- expCount (int) – >= 0 = Number of expression tags in exp_tags array -1 = all dimensions of the sketch
- expTags (list of Tag) – exp_countArray of expression tags of which the dimensions need to be displayed. (is ignored if count
- viewOption (int) – Option for the view, the constants are in uf_disp.h: UF_DISP_ALL_VIEWS_BUT_DRAWING UF_DISP_VIEW_OF_LAST_CURSOR UF_DISP_ALL_ACTIVE_VIEWS UF_DISP_WORK_VIEW_ONLY
- colorOption (int) – Option for the color, the constants are in uf_disp.h: UF_DISP_USE_SYSTEM_COLOR UF_DISP_USE_BACKGROUND_COLOR UF_DISP_USE_ORIGINAL_COLOR UF_DISP_USE_SPECIFIED_COLOR
- color (int) – Color used to display the dimensions if color_option= UF_DISP_USE_SPECIFIED_COLOR. Use the color constants listed in uf_obj.h.
License requirements: None