NXOpen.UF.Disp.DisplayOgpArc¶
-
Disp.
DisplayOgpArc
()¶ Refer to UF_DISP_display_ogp_arc for documentation.
Signature:
DisplayOgpArc(viewTag, orientation, startAngle, endAngle, center, radius)
Parameters: - viewTag (Tag) – Tag of the view in which the arc is to be rendered
- orientation (list of float) – The rotation matrix of the arc (relative to the Work Part Absolute Coordinate System). The matrix must be ortho-normal. If necessary, use UF_MTX3_initialize to create the matrix from X and Y vectors.
- startAngle (float) – Start angle in radians; the zero degree vector is the positive x-axis of the space described by the orientation matrix.
- endAngle (float) – End angle in radians; the zero degree vector is the positive x-axis of the space described by the orientation matrix.
- center (list of float) – The arc center in the coordinate system of the arc (as defined by “orientation” above).
- radius (float) – The radius of the arc (Work Part Absolute units)
License requirements: None