NXOpen.UF.Disp.AskWorkPartMaterialLwaUserAreaData¶
-
Disp.
AskWorkPartMaterialLwaUserAreaData
()¶ Refer to UF_DISP_ask_work_part_material_lwa_user_area_data for documentation.
Signature:
AskWorkPartMaterialLwaUserAreaData(materialTag, attributeStringKey)
Parameters: - materialTag (Tag) – the tag of the material to get the lwa user area data
- attributeStringKey (str) – key to identify which data in the lwa user data area to get NOTE max key length is 31
Returns: return the user area data specified by the attribute_string_key
Return type: str
License requirements: None