NXOpen.UF.CutLevels.SetRangeType¶
-
CutLevels.
SetRangeType
()¶ Refer to UF_CUT_LEVELS_set_range_type for documentation.
Signature:
SetRangeType(operationTag, rangeType)
Parameters: - operationTag (Tag) – The tag of the operation for which thecut levels are defined.
- rangeType (
NXOpen.UF.Param.ClvRangeType
Refer to UF_PARAM_clv_range_type_t for documentation.) – The range type to be set.
Returns: If the data structure created bya call to UF_CUT_LEVELS_load is passed in, then it will be updated to reflect the changes from the new range type. If NULL is passed in, then the argument is ignored.
Return type: NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None