UF_PARAM_regen_e (view source)
Defined in: uf_param.h
Also known as:
Overview
Typedefs
These are the available options for a parameters regeneration type. They
inidicate what must be regenerated if the parameter changes value.
Data Members
UF_PARAM_REGEN_NONE
UF_PARAM_REGEN_POST
UF_PARAM_REGEN_PATH
UF_PARAM_REGEN_ALL
UF_PARAM_status_e (view source)
Defined in: uf_param.h
Also known as:
Overview
These are the various states an object's parameter inheritence
can be in during run time.
Data Members
UF_PARAM_DEFAULT
UF_PARAM_INHERITED
UF_PARAM_OVERRIDDEN
UF_PARAM_INVALID_INDEX
UF_PARAM_type_e (view source)
Defined in: uf_param.h
Also known as:
Overview
These are the available data types that a parameter may be.
LENGTH signifies that the value should be expressed based upon the
units of the part, i.e., inch or mm. VLA signifies that it is an
array with a variable number of elements (currently not supported
in UFUN). 2D and 3D signify 2 doubles and 3 doubles, respectively.
Data Members
UF_PARAM_TYPE_LOGICAL
UF_PARAM_TYPE_CHAR
UF_PARAM_TYPE_SHORT
UF_PARAM_TYPE_INT
UF_PARAM_TYPE_POINTER
UF_PARAM_TYPE_FLOAT
UF_PARAM_TYPE_DOUBLE
UF_PARAM_TYPE_BYTE
UF_PARAM_TYPE_DATE
UF_PARAM_TYPE_TAG
UF_PARAM_TYPE_STRING
UF_PARAM_TYPE_2D
UF_PARAM_TYPE_3D
UF_PARAM_TYPE_VLA_REAL
UF_PARAM_TYPE_VLA_INT
UF_PARAM_TYPE_VLA_TAG
UF_PARAM_TYPE_DOUBLE_LENGTH
UF_PARAM_TYPE_2D_LENGTH
UF_PARAM_TYPE_3D_LENGTH
UF_PARAM_TYPE_VLA_LENGTH
UF_PARAM_TYPE_VLA_STRING
UF_PARAM_TYPE_OBJECT
UF_PARAM_TYPE_VLA_LENGTH_COMPOSITE
UF_PARAM_TYPE_LAST