NXOpen.UF.Assem.McArrayData Structure¶
NXOpen.UF.Assem.McArrayData is an alias for NXOpen.UF.AssemMcArrayData_Struct
-
class
NXOpen.UF.
AssemMcArrayData_Struct
¶ Bases:
object
Refer to UF_ASSEM_mc_array_data_s for documentation.
Fields
NXOpen.UF.AssemMcArrayData_Struct.ArraySubtype |
A flag indicating which type of array this is. |
NXOpen.UF.AssemMcArrayData_Struct.MasterComponent |
The tag of the master component for this array |
NXOpen.UF.AssemMcArrayData_Struct.TemplateComponent |
The tag of the template component for this array. |
NXOpen.UF.AssemMcArrayData_Struct.Dimensions |
An array of expression tags which determine the size of the array. |
NXOpen.UF.AssemMcArrayData_Struct.AxisDefinitions |
The solid entities (faces, datums, etc) which determine the direction of the array. |
NXOpen.UF.AssemMcArrayData_Struct.Offsets |
An array of expression tags which determine the spacing between array elements. |
NXOpen.UF.AssemMcArrayData_Struct.ArrayName |
The name of the array object. |