NXOpen.UF.AssemMcArrayData_Struct.AxisDefinitions¶
-
AssemMcArrayData_Struct.
AxisDefinitions
¶ The solid entities (faces, datums, etc) which determine the direction of the array. For linear arrays, the first element defines the X direction, and the second the Y direction. For one dimensional linear arrays, the second element will be NULL. For circular arrays, the first element is the central axis, and the second is NULL. If these solid objects are in component part files, you should pass in their occurrences in the assembly that contains the array.