UnusedFileManagementBuilder Class¶
-
class
NXOpen.Tooling.
UnusedFileManagementBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.UnusedFileManagementBuilder
Unused File Management is to manage the unused files of the project.To create a new instance of this class, use
NXOpen.Tooling.UnusedFileManagementCollection.CreateUnusedFileManagementBuilder()
Default values.
Property Value ListDir ProjectDirectory SelectAll 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ListDir | Returns or sets the listed directory. |
SelectAll | Returns or sets the select all option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UnusedFileManagementBuilderFileDirectory Enumeration | the unused file location. |
Property Detail¶
ListDir¶
-
UnusedFileManagementBuilder.
ListDir
¶ Returns or sets the listed directory.
-------------------------------------
Getter Method
Signature
ListDir()
Returns: Return type: NXOpen.Tooling.UnusedFileManagementBuilderFileDirectory
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ListDir(listDir)
Parameters: listDir ( NXOpen.Tooling.UnusedFileManagementBuilderFileDirectory
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SelectAll¶
-
UnusedFileManagementBuilder.
SelectAll
¶ Returns or sets the select all option.
-------------------------------------
Getter Method
Signature
SelectAll()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectAll(selectAll)
Parameters: selectAll (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
UnusedFileManagementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.