UnusedFileManagementBuilderFileDirectory Enumeration

NXOpen.Tooling.UnusedFileManagementBuilder.FileDirectory is an alias for NXOpen.Tooling.UnusedFileManagementBuilderFileDirectory

class NXOpen.Tooling.UnusedFileManagementBuilderFileDirectory

Bases: object

the unused file location.

Enum Members

Enum Member Enum Member Description
ProjectDirectory
project directory
RecycleBin
recycle bin
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.