TrimSolidBuilder Class¶
-
class
NXOpen.Tooling.
TrimSolidBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard trim solid management builder, trims bounding box body with region, subtract bounding box with workpiece or keep region and box.
To create a new instance of this class, use
NXOpen.Tooling.TrimSolidCollection.CreateTrimSolidBuilder()
Default values.
Property Value ActionType Trim ChangeBoxSize 1 Clearance.Value 0.1 (millimeters part), 0.004 (inches part) RemoveParameter 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ActionType | Returns or sets the action type of trim, subtract or just keep the region and the bounding box. |
ChangeBoxSize | Returns or sets the option to change the created boundbox size |
Clearance | Returns the single side clearance value of the bounding box. |
RegionFaces | Returns the region faces to create trim solid. |
RemoveParameter | Returns or sets the option to remove parameter of the trim solid body |
SelectBoundBox | Returns the selected bounding box. |
SelectLinkTarget | Returns the component that the trimmed body is linked to. |
SheetBody | Returns the sheet body to create trim solid. |
Tag | Returns the Tag for this object. |
TaggedFaces | Returns the faces with the defined attribute to create trim solid. |
TrimDirection | Returns or sets the trim body side. |
Type | Returns or sets the type to select face, sheet body or manufacturing faces to trim the bounding box. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateBoundBox | Creates the bounding box. |
CreateToolingBox | Creates the tooling box. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InsideBoundBox | The faces inside the bounding box. |
InsideCrossBoundBox | The faces inside/cross the bounding box. |
SetBoundBox | Sets the bounding box tag. |
SetManualBody | Sets the manually selected target body. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimSolidBuilderTrimSolidAction Enumeration | represents the action to create trim solid. |
TrimSolidBuilderTypes Enumeration | represents the option to select face or sheet body or manufacturing faces to trim the bounding box. |
Property Detail¶
ActionType¶
-
TrimSolidBuilder.
ActionType
¶ Returns or sets the action type of trim, subtract or just keep the region and the bounding box.
-------------------------------------
Getter Method
Signature
ActionType()
Returns: Return type: NXOpen.Tooling.TrimSolidBuilderTrimSolidAction
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
ActionType(actionType)
Parameters: actionType ( NXOpen.Tooling.TrimSolidBuilderTrimSolidAction
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ChangeBoxSize¶
-
TrimSolidBuilder.
ChangeBoxSize
¶ Returns or sets the option to change the created boundbox size
-------------------------------------
Getter Method
Signature
ChangeBoxSize()
Returns: Return type: bool New in version NX8.0.18.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChangeBoxSize(changeBoxSize)
Parameters: changeBoxSize (bool) – New in version NX8.0.18.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Clearance¶
-
TrimSolidBuilder.
Clearance
¶ Returns the single side clearance value of the bounding box.
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RegionFaces¶
-
TrimSolidBuilder.
RegionFaces
¶ Returns the region faces to create trim solid.
-------------------------------------
Getter Method
Signature
RegionFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RemoveParameter¶
-
TrimSolidBuilder.
RemoveParameter
¶ Returns or sets the option to remove parameter of the trim solid body
-------------------------------------
Getter Method
Signature
RemoveParameter()
Returns: Return type: bool New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
RemoveParameter(removeParameter)
Parameters: removeParameter (bool) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectBoundBox¶
-
TrimSolidBuilder.
SelectBoundBox
¶ Returns the selected bounding box.
-------------------------------------
Getter Method
Signature
SelectBoundBox()
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectLinkTarget¶
-
TrimSolidBuilder.
SelectLinkTarget
¶ Returns the component that the trimmed body is linked to.
-------------------------------------
Getter Method
Signature
SelectLinkTarget()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SheetBody¶
-
TrimSolidBuilder.
SheetBody
¶ Returns the sheet body to create trim solid.
-------------------------------------
Getter Method
Signature
SheetBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TaggedFaces¶
-
TrimSolidBuilder.
TaggedFaces
¶ Returns the faces with the defined attribute to create trim solid.
-------------------------------------
Getter Method
Signature
TaggedFaces()
Returns: Return type: NXOpen.SelectFaceList
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TrimDirection¶
-
TrimSolidBuilder.
TrimDirection
¶ Returns or sets the trim body side.
-------------------------------------
Getter Method
Signature
TrimDirection()
Returns: Return type: bool New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
TrimDirection(trimDirection)
Parameters: trimDirection (bool) – New in version NX7.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Type¶
-
TrimSolidBuilder.
Type
¶ Returns or sets the type to select face, sheet body or manufacturing faces to trim the bounding box.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.TrimSolidBuilderTypes
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.TrimSolidBuilderTypes
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CreateBoundBox¶
-
TrimSolidBuilder.
CreateBoundBox
¶ Creates the bounding box.
Signature
CreateBoundBox()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CreateToolingBox¶
-
TrimSolidBuilder.
CreateToolingBox
¶ Creates the tooling box.
Signature
CreateToolingBox()
Returns: the bounded box body Return type: NXOpen.Body
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
InsideBoundBox¶
-
TrimSolidBuilder.
InsideBoundBox
¶ The faces inside the bounding box.
Signature
InsideBoundBox()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
InsideCrossBoundBox¶
-
TrimSolidBuilder.
InsideCrossBoundBox
¶ The faces inside/cross the bounding box.
Signature
InsideCrossBoundBox()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetBoundBox¶
-
TrimSolidBuilder.
SetBoundBox
¶ Sets the bounding box tag.
Signature
SetBoundBox(block)
Parameters: block ( NXOpen.Body
) – the bounding box block bodyNew in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetManualBody¶
-
TrimSolidBuilder.
SetManualBody
¶ Sets the manually selected target body.
Signature
SetManualBody(block)
Parameters: block ( NXOpen.Body
) – the manually selected target bodyNew in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
TrimSolidBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.