TrimSolidBuilderTrimSolidAction Enumeration¶
NXOpen.Tooling.TrimSolidBuilder.TrimSolidAction is an alias for NXOpen.Tooling.TrimSolidBuilderTrimSolidAction
-
class
NXOpen.Tooling.
TrimSolidBuilderTrimSolidAction
¶ Bases:
object
represents the action to create trim solid.
Enum Members
Enum Member Enum Member Description Trim Action to do trim.Subtract Action to do subtract.KeepBoxandRegion Action to keep box and region.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-