TrimRegionBuilder Class¶
-
class
NXOpen.Tooling.
TrimRegionBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies.
Optionally creates output trimmed sheet body as a patch surface. To create a new instance of this class, use
NXOpen.Tooling.TrimRegionCollection.CreateTrimRegionBuilder()
Default values.
Property Value AsPatchSurface 1 BoundaryType BodyCurve RegionType Keep New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AsPatchSurface | Returns or sets the value of option, which specifies whether to set the result region as patch surface or not. |
BodyColor | Returns or sets the color value of patch surface body. |
BoundaryBody | Returns the selection of boundary body to extract region faces, which are used for create intersection curves with target. |
BoundaryType | Returns or sets the value of boundary type option, which specifies to use body or edge/curve as boundary object. |
LoopCollector | Returns the loop collector to collect the traverse loops. |
RegionPoint | Returns the selection of region point, which will be kept or discarded as the result of trim region. |
RegionType | Returns or sets the value of the option, which specifies to keep or discard the selected region. |
Tag | Returns the Tag for this object. |
TargetBody | Returns the selection of target to create trim region, body type only. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetColorValue | Returns the value of surface patch color. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetColorValue | Sets the value of surface patch color. |
SetTraverseEdges | Sets the edges from traverse loop to builder data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimRegionBuilderBoundaryOption Enumeration | represents the boundary type option, body/curve type or traverse type. |
TrimRegionBuilderRegionOption Enumeration | represents the option to keep or discard the selected region. |
Property Detail¶
AsPatchSurface¶
-
TrimRegionBuilder.
AsPatchSurface
¶ Returns or sets the value of option, which specifies whether to set the result region as patch surface or not.
-------------------------------------
Getter Method
Signature
AsPatchSurface()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AsPatchSurface(asPatchSurface)
Parameters: asPatchSurface (bool) – New in version NX7.5.0.
License requirements: None.
BodyColor¶
-
TrimRegionBuilder.
BodyColor
¶ Returns or sets the color value of patch surface body.
-------------------------------------
Getter Method
Signature
BodyColor()
Returns: the color index Return type: Id New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyColor(patchColor)
Parameters: patchColor (Id) – the color index New in version NX8.0.1.
License requirements: None.
BoundaryBody¶
-
TrimRegionBuilder.
BoundaryBody
¶ Returns the selection of boundary body to extract region faces, which are used for create intersection curves with target.
-------------------------------------
Getter Method
Signature
BoundaryBody()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
BoundaryType¶
-
TrimRegionBuilder.
BoundaryType
¶ Returns or sets the value of boundary type option, which specifies to use body or edge/curve as boundary object.
-------------------------------------
Getter Method
Signature
BoundaryType()
Returns: Return type: NXOpen.Tooling.TrimRegionBuilderBoundaryOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryType(boundaryType)
Parameters: boundaryType ( NXOpen.Tooling.TrimRegionBuilderBoundaryOption
) –New in version NX7.5.0.
License requirements: None.
LoopCollector¶
-
TrimRegionBuilder.
LoopCollector
¶ Returns the loop collector to collect the traverse loops.
-------------------------------------
Getter Method
Signature
LoopCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
RegionPoint¶
-
TrimRegionBuilder.
RegionPoint
¶ Returns the selection of region point, which will be kept or discarded as the result of trim region.
-------------------------------------
Getter Method
Signature
RegionPoint()
Returns: Return type: NXOpen.RegionPointList
New in version NX7.5.0.
License requirements: None.
RegionType¶
-
TrimRegionBuilder.
RegionType
¶ Returns or sets the value of the option, which specifies to keep or discard the selected region.
-------------------------------------
Getter Method
Signature
RegionType()
Returns: Return type: NXOpen.Tooling.TrimRegionBuilderRegionOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionType(regionType)
Parameters: regionType ( NXOpen.Tooling.TrimRegionBuilderRegionOption
) –New in version NX7.5.0.
License requirements: None.
TargetBody¶
-
TrimRegionBuilder.
TargetBody
¶ Returns the selection of target to create trim region, body type only.
-------------------------------------
Getter Method
Signature
TargetBody()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetColorValue¶
-
TrimRegionBuilder.
GetColorValue
¶ Returns the value of surface patch color.
Signature
GetColorValue()
Returns: a tuple Return type: A tuple consisting of (redValue, greenValue, blueValue). redValue is a float. red value between 0 and 1 greenValue is a float. green value between 0 and 1 blueValue is a float. blue value between 0 and 1 New in version NX7.5.0.
License requirements: None.
SetColorValue¶
-
TrimRegionBuilder.
SetColorValue
¶ Sets the value of surface patch color.
Signature
SetColorValue(redValue, greenValue, blueValue)
Parameters: - redValue (float) – red value between 0 and 1
- greenValue (float) – green value between 0 and 1
- blueValue (float) – blue value between 0 and 1
New in version NX7.5.0.
License requirements: None.
SetTraverseEdges¶
-
TrimRegionBuilder.
SetTraverseEdges
¶ Sets the edges from traverse loop to builder data.
Signature
SetTraverseEdges(traverseEdges)
Parameters: traverseEdges (list of NXOpen.NXObject
) – the selected edgesNew in version NX7.5.0.
License requirements: None.
Validate¶
-
TrimRegionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.