TrimRegionBuilderBoundaryOption Enumeration¶
NXOpen.Tooling.TrimRegionBuilder.BoundaryOption is an alias for NXOpen.Tooling.TrimRegionBuilderBoundaryOption
-
class
NXOpen.Tooling.
TrimRegionBuilderBoundaryOption
¶ Bases:
object
represents the boundary type option, body/curve type or traverse type.
Enum Members
Enum Member Enum Member Description BodyCurve select body/edge/curve as boundary objectTraverse use traverse loop to select boundary object-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-