StripLayoutBuilder Class¶
-
class
NXOpen.Tooling.
StripLayoutBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.StripLayoutBuilder
This class is for Strip Layout Design UITo create a new instance of this class, use
NXOpen.Tooling.StripLayoutCollection.CreateStripLayoutBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
FromStation | Returns or sets the From Station type on the Layout group of Strip Layout Design dialog |
Tag | Returns the Tag for this object. |
ToStation | Returns or sets the To Station type on the Layout group of Strip Layout Design dialog |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StripLayoutBuilderFromStationType Enumeration | Specifies the option of From Station for layout |
StripLayoutBuilderToStationType Enumeration | Specifies the option of To Station for layout |
Property Detail¶
FromStation¶
-
StripLayoutBuilder.
FromStation
¶ Returns or sets the From Station type on the Layout group of Strip Layout Design dialog
-------------------------------------
Getter Method
Signature
FromStation()
Returns: Returns the from station value Return type: NXOpen.Tooling.StripLayoutBuilderFromStationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromStation(fromStation)
Parameters: fromStation ( NXOpen.Tooling.StripLayoutBuilderFromStationType
) – Sets the from station valueNew in version NX6.0.0.
License requirements: None.
ToStation¶
-
StripLayoutBuilder.
ToStation
¶ Returns or sets the To Station type on the Layout group of Strip Layout Design dialog
-------------------------------------
Getter Method
Signature
ToStation()
Returns: Returns the to station value Return type: NXOpen.Tooling.StripLayoutBuilderToStationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToStation(toStation)
Parameters: toStation ( NXOpen.Tooling.StripLayoutBuilderToStationType
) – Sets the to station valueNew in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
StripLayoutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.